Showing 8,481 - 8,490 of 9,888 results

Page 849 of 989
  • Resetting the device

    Unica - Connected Wireless Switch 1-gang/2-gang – Wiser Home Device user guide

    (< 0,5 s) the push button (A) 3 times and then press and hold the push button (> 10 s). After 10 s, the status LED blinks red. Release the push button. The status LED stops blinking upon successful reset of the device. The Wireless switch restarts and blinks green for few seconds. After reset, the status LED turns off. All configuration data, user data, and network data are deleted. Assemble the rocker on the Wireless switch.
  • Troubleshooting

    Ovalis - Connected Wireless Switch 1-gang/2-gang – Wiser Home Device user guide

    Troubleshooting Troubleshooting Troubleshooting Symptom Possible cause Solution LED blinks red. The Wireless switch battery is low or drained. Replace the Wireless switch battery. A notification pop-up will appear in the app. The Wireless switch displays offline in the app. The Wireless switch
  • Resetting the device

    Ovalis - Connected Wireless Switch 1-gang/2-gang – Wiser Home Device user guide

    (< 0,5 s) the push button (A) 3 times and then press and hold the push button (> 10 s). After 10 s, the status LED blinks red. Release the push button. The status LED stops blinking upon successful reset of the device. The Wireless switch restarts and blinks green for few seconds. After reset, the status LED turns off. All configuration data, user data, and network data are deleted. Assemble the rocker on the Wireless switch.
  • Resetting the Device in Quick Home Connect

    Odace - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

  • Restablecimiento del dispositivo en Quick Home Connect

    Unica - regulador LED universal de pulsación conectado – Guía del usuario del dispositivo Wiser Home

    Restablecimiento del interruptor inalámbrico Restablecimiento del regulador de pulsador Cuando el reinicio se realiza correctamente, el interruptor inalámbrico y el dispositivo vuelven a los valores por defecto de fábrica. Integración en el sistema Wiser Si deseas integrar los dispositivos en el sistema
  • Configuration du comportement des témoins LED

    Odace - Interrupteur à relais 10 A connecté – Guide de l'utilisateur du dispositif Wiser Home

  • Troubleshooting

    Odace - Connected Universal Push-button Dimmer LED – Wiser Home Device User Guide

    . Reduce load. Change load. Check wiring between the push button and the Dimmer. Flickering at minimum brightness. Increase minimum brightness (if flickering still persists, install a 31LCDA load correction device). Change the load (if the minimum brightness is insufficient). Set to RL LED mode
  • Fehlerbehebung

    System M und System D - Connected SCHUKO-Steckdose 16 A – Wiser Home Geräte-Benutzerhandbuch

  • Comprobación del historial del dispositivo

    Detector de humo inalámbrico Wiser – Guía del usuario del dispositivo Wiser Home

    en la nube. Cuando se pierda la conexión a la nube, desaparecerá el historial del dispositivo. En la pestaña Control, pulse Todos los dispositivos o la pestaña de la habitación en la que se encuentra la alarma de humo. En la página del panel de control del dispositivo, pulse Historial. En la página Historial, puede ver la fecha, la hora y el tipo de alarma detectada. El historial del dispositivo puede almacenarse durante un máximo de 90 días.
  • Tratamiento de problemas con el código QR

    Wiser Home – Guía del usuario del sistema (España y Portugal)

    continúe con Añadir un dispositivo. Si el código QR es incorrecto, aparece el mensaje Código QR escaneado incorrecto. Pulse No puedo escanear el código QR y seleccione una de las siguientes opciones: (E): Introduzca la dirección MAC/EUI-64 y el código de instalación y, a continuación, pulse Conectar. La
Page 849 of 989