DUG_Unica-Wireless Switch_WH-05

Resetting the device

You can reset the Wireless switch to factory default manually under the following conditions:
  • When the Hub is replaced.

  • When Switching from 1-gang to 2-gang or vice versa.

To reset the Wireless switch:

  1. Remove the rocker.
  2. Short press (< 0,5 s) the push button (A) 3 times and then press and hold the push button (> 10 s).
    After 10 s, the status LED blinks red.
  3. Release the push button.
    • The status LED stops blinking upon successful reset of the device. 

    • The Wireless switch restarts and blinks green for few seconds. After reset, the status LED turns off.

    NOTE: All configuration data, user data, and network data are deleted.

  4. Assemble the rocker on the Wireless switch.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?