Showing 921 - 930 of 1,449 results

Page 93 of 145
  • Affichages LED dans Quick Home Connect

    Odace - Poussoir variateur connecté universel LED 2 fils / 3 fils – Wiser Home Dispositif Guide de l'utilisateur

    Affichages LED dans Quick Home Connect Affichages LED dans Quick Home Connect Affichages LED dans Quick Home Connect Appairage de l’appareil dans Quick Home Connect Action de l’utilisateur Affichage LED État Appuyez brièvement 5 fois de suite rapidement sur le bouton-poussoir. Le voyant clignote en vert une fois par seconde. Le mode d’appairage est actif pendant 60 secondes. Lorsque l’appairage est terminé, le voyant arrête de clignoter.
  • Création d’un automatisme

    Capteur de mouvement Wiser – Guide de l'utilisateur de l’appareil Wiser Home

    , tel que l’ouverture d’un volet ou la détection d’un mouvement par un capteur de mouvement. Mode Absence (activez ou désactivez) : Le mode Absence peut également déclencher un automatisme pour allumer les lumières, fermer les volets, etc. Reportez-vous à la rubrique Mode Absence dans le Guide de
  • Pairing 2-gang Wireless switch with 2 Micro Module Dimmers (Pucks)

    Wiser Micro Module Dimmer – Wiser Home Device user guide

    pairing mode. The pairing mode will be active for about a minute. Short press the upper right push button 5 times in quick succession on the Wireless switch. The status LED blinks green. HAZARD OF ELECTRIC SHOCK Observe the regulations for working on live parts. Only actuate the device buttons using
  • Creating a Schedule/Event

    Wiser Radiator Thermostat – Wiser Home Device user guide

    schedule, the Frost Protection mode is activated when the schedule begins.In the frost protection mode, the system maintains the room temperature at 5 °C. Set time (for example 12:00). A maximum of 8 events can be created per day. You can tap to copy the schedule from one day to other days or copy the
  • Creating a Schedule/Event

    Odace - Connected Thermostat 2 A – Wiser Home Device user guide

    schedule, the Frost Protection mode is activated when the schedule begins.In the frost protection mode, the system maintains the room temperature at 5 °C. Set time (for example 12:00). A maximum of 8 events can be created per day. You can tap to copy the schedule from one day to other days or copy the
  • Creating a Schedule/Event

    Renova - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    schedule, the Frost Protection mode is activated when the schedule begins.In the frost protection mode, the system maintains the room temperature at 5 °C. Set time (for example 12:00). A maximum of 8 events can be created per day. You can tap to copy the schedule from one day to other days or copy the
  • Troubleshooting

    Wiser 16 A Relay for Temperature Control – Wiser Home Device user guide

    Troubleshooting Troubleshooting Troubleshooting Symptom Possible cause Solution The relay displays offline in the app or the LED flashing or solid red. Weak or no signal between the Wiser Hub and the relay. The relay is working in degraded mode. Check Hub is online. Check signal strength. The relay is flashing green. Emergency heat is active. Press the button to cancel the emergency heat function.
  • Réinitialisation du dispositif

    Wiser micromodule pour interrupteur – Guide de l'utilisateur du dispositif Wiser Home

    Réinitialisation du dispositif Réinitialisation du dispositif Réinitialisation du dispositif Sélectionnez l’une des options pour réinitialiser l’équipement en mode par défaut : Appuyez brièvement 3 fois sur le bouton Setup/Reset, puis appuyez une fois sur le bouton de configuration/réinitialisation
  • Dépannage

    Wiser Actionneur de Chauffage électrique pour la commande de température – Guide de l’utilisateur de l’appareil

    Dépannage Dépannage Dépannage Symptôme Cause possible Solution L'actionneur affiche « Hors ligne » dans l’application ou la LED clignote ou reste allumée en rouge. Signal faible ou inexistant entre la passerelle Wiser et le relais. L'actionneur fonctionne en mode dégradé. Vérifiez que la passerelle
  • Affichages LED dans Quick Home Connect

    Wiser micromodule pour variateur – Guide de l'utilisateur de l’appareil Wiser Home

    Affichages LED dans Quick Home Connect Affichages LED dans Quick Home Connect Affichages LED dans Quick Home Connect Appairage de l’appareil dans Quick Home Connect Action de l’utilisateur Affichage LED État Appuyez brièvement 5 fois de suite rapidement sur le bouton-poussoir. Le voyant clignote en vert une fois par seconde. Le mode d’appairage est actif pendant 60 secondes. Lorsque l’appairage est terminé, le voyant arrête de clignoter.
Page 93 of 145