DUG_ Connected Motion Sensor Dimmer_WH-01

Setting the motion detection timer

You can set the motion detection timer.
  1. On the Home screen, tap .
  2. Tap Devices > Lights > Motion Dimmer > Motion Detection Timer and select any one of the following options:
    • 15 sec

    • 30 sec

    • 45 sec

    • 1 min

    • 5 min

    • Specific time

    TIP: The Specific Time allows you to manually define how long the light should remain On after motion is detected. The maximum time limit you can add is up to 59 min 59 sec.
    NOTE: The motion detection timer is set to 5 min by default.
  3. On the top-right screen, tap Set.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?