Configuring the device
|
A |
Device Name: Tap to change the name of the device. |
|
B |
Location: Tap to assign the Dimmer to any room (such as living room, bedroom, kitchen etc). Refer to Setting the device location for more details on how to set the location. |
|
C |
RL-LED Mode: You can improve the dimming quality in the app if you have problems with light flickering. Tap the toggle switch to enable the RL-LED Mode. NOTE: Refer to Technical Data for more information.
|
|
D |
LED Indicator Behaviour: Tap to set the LED indicator behaviour of the dimmer as per your preference. Refer to Setting up the LED Indicator Behaviour for detailed information on each options. |
|
E |
Power On Behaviour: Tap to set the default brightness level of the dimmer when it is turned on. Refer to Setting up the Power On Behaviour for detailed information on each options. |
|
F |
Minimum Brightness and Maximum Brightness: This setting lets
you set limits on the maximum and minimum brightness of the connected
load. This is done to avoid flickering and switching off the LED. |
|
G |
Identify: Tap
to identify the device. The status LED blinks red and connected lighting
devices blinks On/Off, upon successful identification of the dimmer. |
|
H |
Delete: Tap to remove the device from the system. NOTE:
|
|
J |
Zigbee Signal Strength Indicator: Zigbee Signal Strength indicator which displays the current signal strength of the device. |