Using the device
The Device Control Screen allows you to switch ON/OFF the device and control various settings.
On the Control tab, select the dimmer and the control screen shows the options below.
|
A |
Drag the sliding bar up/down to increase/ decrease the brightness. |
|
B |
Tap to manually turn the device ON/OFF. |
|
C |
Tap to redirect you to the Schedule screen, where you can create a schedule. For more information, refer to the Setting up a schedule topic. |
|
D |
Tap to add the device to the Favourite devices section on the Home screen. To know more about Favourite, refer to Managing Favourites in the respective System User Guide |
|
E |
Tap to control various settings from the Device Settings screen. For more information, refer to the Configuring the device topic. |