Pairing the device with the Wiser Hub

Using the Wiser Home app, pair your Boiler Relay with the Wiser system to access and control the Boiler Relay.
To pair the Boiler Relay:
  1. On the Home screen, tap .
  2. Tap Devices > and tap Climate > Boiler Relay.
    TIP: You can also navigate by tapping Control tab > > Climate > Boiler Relay.
  3. Tap Scan QR code and allow the Wiser Home app to access your camera. Then, scan the QR code located on the device.
    NOTE: If you are unable to find the correct QR code, tap I can't find the correct QR code to pair the device manually and proceed to step 4.

    If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options:

    • (A): Enter the Mac Address/EUI-64 and Install Code, then tap Connect. The app will verify if the Mac Address/EUI-64 and Install code are valid.

    • (B): Tap this option if you are unable to find the Mac Address/EUI-64 and Install code.

  4. Once the device is validated, tap Next, press and hold the Setup button for more than 2 s until the LED flashes green/amber.
    Wait for a few seconds until the LED turns green and the app confirms that the relay is joined.
    TIP: If the device fails to join, then the LED glows red.

    After you pair the device, a success screen appears with the following options:

    • + Add New Device: Tap to continue pairing more devices.

    • Start Using Your Device: Tap to start using the paired device.

    NOTE: The success screen appears only if you are logged in as a Home Owner.

  5. Enter the Boiler Relay name and tap Next.
  6. On the Boiler Relay Setup page, select the Control Type:
    • Relay :

      If Relay is selected, choose one of the following Heat Source Type:

      • Gas Boiler (Default)

      • Electric Boiler

      • Oil Boiler

      • Heat Pump

    • OpenTherm: If selected OpenTherm (interfacing cable between Boiler Relay and Boiler) then the setup is completed.
    TIP: Depending on the boiler interface choose the correct Relay or OpenTherm ®.
The Boiler Relay is now listed on the Control tab under the All and the specific room tabs.
NOTE: If you only have a single device in the Wiser System, the Control tab will not be visible. All functions will be accessible through the Home screen.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?