DUG_Wiser Plug_WH-10

Resetting the device

To reset the device, follow these steps based on your device:
  1. Ensure that the Plug is installed in a wall socket.

  2. Press and hold the ON/OFF button.

  3. In five seconds the LED will flash blue six times then go out. The Plug is now reset.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.