DUG_Wiser Micro Module Blind_Pacific_WSE-00

Manual operation

When the module is connected to a mechanical double push-button switch, the shutter can be controlled manually.

  • Short press the push button once, the shutter opens/closes gradually.

  • Press and hold the push button, the shutter opens/closes fully.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?