Zone Selective Interlocking Test
Zone Selective Interlocking Test Requirements
The system should be tested upon initial start-up and:
-
in accordance with a facility maintenance schedule;
-
if any of the components in the system are replaced;
-
if any work is done in the area of the system wiring;
-
if required per the installation requirements.
Zone Selective Interlocking Test Necessary Tools
The following is needed to perform a zone selective interlocking test:
|
Downstream Circuit Breaker |
Upstream Circuit Breaker |
||||
|---|---|---|---|---|---|
|
MasterPacT MTZ |
MasterPacT NW |
MasterPacT NT |
PowerPacT P/R |
PowerPacT H/J/L |
|
|
MasterPacT MTZ |
EcoStruxure Power Commission Software |
EcoStruxure Power Commission Software |
EcoStruxure Power Commission Software |
N/A |
N/A |
| Mini B USB Cable Ethernet Patch Cord | Mini B USB Cable Ethernet Patch Cord | Mini B USB Cable Ethernet Patch Cord | |||
|
0614DB2001 User Guide (this document) |
0614DB2001 User Guide (this document) |
0614DB2001 User Guide (this document) |
|||
|
MasterPacT NW |
Full Function Test Kit or Service Interface Kit |
Full Function Test Kit or Service Interface Kit |
N/A |
N/A |
N/A |
|
NHA35975 Full-Function Test
Kit Instruction bulletin. |
NHA35975 Full-Function Test Kit Instruction bulletin. or service interface for MasterPacT NT/NW, ComPacT NS, and PowerPacT P-, R-Frame circuit breakers. User guide: DOCA0170EN |
||||
|
MasterPacT NT |
Full Function Test Kit or Service Interface Kit |
Full Function Test Kit or Service Interface Kit |
Full Function Test Kit or Service Interface Kit |
N/A |
N/A |
|
NHA35975 Full-Function Test
Kit Instruction bulletin. |
NHA35975 Full-Function Test
Kit Instruction bulletin. |
NHA35975 Full-Function Test
Kit Instruction bulletin. |
|||
|
PowerPacT P/R |
Full Function Test Kit or Service Interface Kit |
Full Function Test Kit or Service Interface Kit |
Full Function Test Kit or Service Interface Kit |
Full Function Test Kit or Service Interface Kit |
N/A |
|
NHA35975 Full-Function Test
Kit Instruction bulletin. |
NHA35975 Full-Function Test
Kit Instruction bulletin. |
NHA35975 Full-Function Test
Kit Instruction bulletin. |
NHA35975 Full-Function Test
Kit Instruction bulletin. |
||
|
PowerPacT H/J/L |
UTA tester+ Local Test Utility Software |
UTA tester+ Local Test Utility Software |
UTA tester + Local Test Utility Software |
UTA tester + Local Test Utility Software |
UTA tester + Local Test Utility Software |
|
Refer to the connection procedure and miscellaneous section in the LTU software’s online help. |
Refer to the connection procedure and miscellaneous section in the LTU software’s online help. |
Refer to the connection procedure and miscellaneous section in the LTU software’s online help. |
Refer to the connection procedure and miscellaneous section in the LTU software’s online help. |
Refer to the connection procedure and miscellaneous section in the LTU software’s online help. |
|
Zone Selective Interlocking Test
|
1 |
To perform the ZSI test: use a USB cable to connect the PC to the MicroLogic X control unit of the downstream circuit breaker. NOTE: For the downstream breaker other than MasterPacT MTZ , refer to Zone Selective Interlocking Test Necessary Tools for
Zone Selective Interlocking test tools and test procedure reference
documents.
|
||
|
2 |
On the PC, open the EcoStruxure Power Commission software and click on “Connect to device directly” (A). This will allow the user access to the MasterPacT MTZ circuit breaker through the commissioning tool. |
||
|
3 |
In order to perform the test, add upstream circuit breakers to the project. Click on “Devices” (B) to add upstream breaker(s). NOTE: To perform the ZSI test and to generate the
project report with the test details, you must have downstream and
upstream circuit breakers in the same EPC project.
|
|
|
|
4 |
To check zone-selective interlocking (ZSI) operation between the USB-connected circuit breaker (step 3 above), and one or more upstream ZSI-connected circuit breakers that are connected to the same communications network, connect the PC to the communications network using an Ethernet cable. Auto-discover the devices and select the ZSI connected devices (C). NOTE: To discover circuit breakers that are connected through
IFM communications modules, add the Modbus device ID for the connected
IFE gateway IP address.
OR Click “ADD MANUALLY” (D) to add one or more devices by entering the IP address (E) and the Modbus device ID if the circuit breakers are connected through IFM communication. NOTE: Range of the IP address can also be used
(for example, 10.179.192.110–120).
Click “FIND DEVICES”. (F). This displays the Devices List with devices discovered in the TCP/IP network. NOTE: If the circuit breakers
are on a different network, then connect the upstream circuit breaker
directly through USB and search for the device via the USB serial.
|
||
|
5 |
Select the upstream circuit breakers to be tested (G) and click “ADD DEVICES” (H) to add them to the project. |
||
|
6 |
Click “CONNECT TO DEVICE” (I) on the device page of the downstream circuit breaker to connect directly through USB. |
||
|
7 |
NOTE: For the upstream device, the tsd and tg tripping delays must not be set to zero because this would make selectivity impossible. Select the “Zone Selective Interlocking Test” option in the device view (J). |
||
|
8 |
Select the upstream circuit breaker/breakers (K) and click “RUN TEST” (L). |
||
|
9 |
The password screen will appear. Enter the password (M) and click on “CONTINUE” (N). NOTE: The default password is
"0000".
|
||
|
10 |
Check if the test has passed. To determine if the test has passed, check if the Isd/Ii and Ig LEDs on the control unit of the upstream circuit breakers are blinking red. |
||
|
11 |
If the test passed click the check icon (O) If the test did not pass click the cross icon
(P) RESULT: Icon selected is highlighted. Click “END TEST” (Q). |
||
|
12 |
Click “CONFIRM” (R) to proceed with “END TEST”. |
||
|
13 |
Click “CLOSE” (S). |
||
|
14 |
Project report can be obtained from the Reports option in Device view. |
||
|
15 |
The Zone-Selective Interlocking (ZSI) test verifies field wiring between multiple circuit breakers connected in a ZSI system. A primary injection test must be done to test the performance of the circuit breaker’s ZSI function. |
||