Final Preparation and Energization
This chapter contains information on how to operate HVL/cc Metal-Enclosed Switchgear.
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Final Operating Checks
Perform the following minimum list of operating tests that before energization:
With all power off, perform the following checks:
-
Operate the grounding switch (if equipped) a minimum of five times and verify that the LDA (if equipped) is functioning properly. (All contact fingers must touch the field shapers when the main switch is in the grounded position.)
-
Operate the load switch a minimum of five times.
-
With the switch in the CLOSE position, verify that the load-side panel cannot be removed (see Removing the Load-side Access Panels).
-
When mechanical interlocks are present for automatic transfer or duplex switching, verify that only one switch will operate at a time.
-
Verify that the CT circuits are not shorted at the terminal block.
-
Replace all devices, doors, and covers before turning on the power to the equipment.
Energization
After the proper testing is complete on the incoming service cables and before the switch is energized, perform the following operations.
-
Open the incoming main switch.
-
Energize the incoming cables.
-
The Live Line Indicators (LLIs) are located on the main source side of the line-up as in Using Live Line Indicators. The LLI is not an indicator of the absence of voltage. As soon as the circuits are energized, the voltage indicator lamps should illuminate.
-
Perform phase sequence tests on equipment with multiple incoming lines. Phase sequence tests can be performed through the test ports on the optional LLIs (see Phase Sequence Testing).
NOTE: Test ports will have a potential of 17–60 V (L-G) depending on version of light head module. -
Close the switch, and the load-side indicators should illuminate.
-
Close the load and feeder circuits, if provided in the line-up, one at a time.
DANGER