Receiving, Handling, and Storage
This chapter contains information regarding the receiving, handling, and storage of HVL/cc Metal-Enclosed Switchgear.
Receiving
Metal-enclosed switchgear is shipped on skids with protective wrapping to help prevent damage during normal transit. Check the packing list against the equipment received to ensure the order and shipments are complete. Claims for shortages or other errors must be made in writing to Schneider Electric within 30 days after receipt of shipment. Failure to do so constitutes unqualified acceptance and a waiver of all such claims by the purchaser.
Upon receipt, immediately inspect the switchgear for damage that may have occurred during transit. If damage is found or suspected, immediately file a claim with the carrier and notify Schneider Electric.
Identification
The rating nameplate is located on the front cover of the operating mechanism. Included on the nameplate is the following information:
-
Factory order number
-
Manufacture date
-
Rated maximum voltage
-
Impulse BIL (kV)
-
Power frequency withstand (kV)
-
Frequency
-
Switch continuous current (A)
-
Main bus ratings
-
Momentary current (kA)
-
Short time current (kA)
-
Fault closing current (kA)
-
Fuse information
Handling
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Switchgear is normally shipped in an upright position. However, single frames may be shipped laying down.
Use care when uncrating, rolling, hoisting, or handling the switchgear.
WARNING |
|---|
|
EQUIPMENT Distortion
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
Lifting Provision-Indoor
Removable lifting angles are provided for inserting hooks to lift each section. Use hooks on angles (see Lifting Provision–Indoor) to properly lift and move indoor metal enclosed switchgear. A minimum of 40 in. (1,016 mm) between the lifting cables assembly and the top of the switchgear is required.
Lifting Provision-Outdoor
Lifting angles are provided for inserting hooks to lift each shipping section. Retain these angles and hardware for use in anchoring outdoor shipping sections (see Anchoring and Joining the Shipping Split Frames and Anchoring Subsequent Indoor Shipping Splits). A minimum of 40 in. (1,016 mm) between the lifting cables assembly and the top of the switchgear is required. Use spreader bars and a hook to the bottom provisions (see Figure 12) to properly lift and move outdoor metal-enclosed switchgear.
Using a Forklift
Use only equipment of proper load range for lifting the switchgear. Review the shipping documentation for the actual weight of the equipment. When an overhead crane is not available, rollers or pipes may be used for moving the switchgear to its location. Forklifts of proper load range may be used (see Handling Using a Forklift). This equipment is shipped up to a maximum of five vertical units or to 75 in. (1,905 mm) wide.
WARNING |
|---|
|
TOP HEAVY LOAD
If lifting the switchgear by forklift, stabilize the shipping
section with a safety strap to reduce the possibility of tipping.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
Storage
If the switchgear is stored before being placed into service, keep it in a clean, dry place that is free from condensing conditions, corrosive elements, and mechanical abuse. Energize the heaters inside the switchgear, or add heat from a separate source, such as a light bulb or blower. Use a minimum of 125 W of heat per vertical section to keep the equipment dry during storage.
Covering the equipment with a tarpaulin may be necessary to help protect it from contaminants or moisture. Do not store indoor units outdoors.
In areas of high humidity, such as installations near oceans or large bodies of water, monitor the equipment closely. If necessary, use additional heat to keep the switchgear dry. Contact the factory if the internal heaters do not adequately prevent condensation for your location or environmental condition.
The drawings below are examples of a typical Application A Indoor and Outdoor Metal-enclosed Switchgear.
Refer to the customer drawings for the actual weights, dimensions, and conduit entry locations. The weights given below are approximate and are not correct for all combinations of gear.
Storage Weights
|
Frame Width (X) |
|||
|---|---|---|---|
|
14.75 in. (375 mm) |
20.00 in. (508 mm) |
29.50 in. (750 mm) |
|
|
Bolt Center (Y) |
13.50 in. (343 mm) |
18.75 in. (476 mm) |
28.25 in. (717 mm) |
|
Unfused Switch |
445 lb. (200 kg) |
485 lb. (218 kg) |
545 lb. (245 kg) |
|
Fused Switch |
480 lb. (216 kg) |
520 lb. (234 kg) |
580 lb. (261 kg) |
|
Transition/Auxiliary Unit |
210 lb. (95 kg) |
250 lb. (160 kg) |
— |
|
VT Compartment |
— |
820 lb. (369 kg) |
875 lb. (394 kg) |
|
CT Compartment |
— |
— |
835 lb. (376 kg) |
2.4–15 kV Switchgear Indoor (NEMA 1 Construction)
Approximate Dimensions and Weights 2.4–15 kV-Indoor
|
Frame Width (X) |
|||
|---|---|---|---|
|
14.75 in. (375 mm) |
20.00 in. (508 mm) |
29.50 in. (750 mm) |
|
|
Bolt Center (Y) |
13.50 in. (343 mm) |
18.75 in. (476 mm) |
28.25 in. (717 mm) |
|
Unfused Switch |
445 lb (200 kg) |
485 lb (218 kg) |
545 lb (245 kg) |
|
Fused Switch |
480 lb (216 kg) |
520 lb (234 kg) |
580 lb (261 kg) |
|
Transition/Auxiliary Unit |
210 lb (95 kg) |
250 lb (160 kg) |
— |
|
VT Compartment |
— |
820 lb (369 kg) |
875 lb (394 kg) |
|
CT Compartment |
— |
— |
835 lb (376 kg) |
2.4–15 kV Switchgear Outdoor (NEMA 3R Construction)
Approximate Dimensions and Weights 2.4–15 kV-Outdoor
|
Frame Width (X) |
|||
|---|---|---|---|
|
14.75 in. (375 mm) |
20.00 in. (508 mm) |
29.50 in. (750 mm) |
|
|
Bolt Center (Y) |
Add 2.25 in. (57 mm) to the total length of the switchgear lineup |
||
|
Unfused Switch |
585 lb. (263 kg) |
655 lb. (295 kg) |
785 lb. (353 kg) |
|
Fused Switch |
629 lb. (278 kg) |
685 lb. (308 kg) |
820 lb. (370 kg) |
|
Transition/Auxiliary Unit |
440 lb. (200 kg) |
450 lb. (205 kg) |
— |
|
VT Compartment |
— |
985 lb. (443 kg) |
1115 lb. (502 kg) |
|
CT Compartment |
— |
— |
1075 lb. (484 kg) |
|
End Panel |
End panels add 90 lb. (40.5 kg) per end unit |
||
25.8–38 kV Switchgear Indoor (NEMA 1 Construction)
Approximate Dimensions and Weights 25.8–38 kV-Indoor
|
Frame Width (X) |
||
|---|---|---|
|
29.50 in. (750 mm) |
39.37 in. (1000 mm) |
|
|
Bolt Center (Y) |
25.76 in. (654 mm) |
35.63 in. (905 mm) |
|
Unfused Switch |
760 lb. (345 kg) |
877 lb. (400 kg) |
|
Fused Switch |
795 lb. (360 kg) |
915 lb. (420 kg) |
|
Transition/Auxiliary Unit |
510 lb. (230 kg) |
625 lb. (280 kg) |
|
VT Compartment |
1090 lb. (495 kg) |
1200 lb. (545 kg |
|
CT Compartment |
1050 lb. (475 kg) |
1160 lb. (525 kg) |
25.8–38 kV Switchgear Outdoor (NEMA 3R Construction)
Approximate Dimensions and Weights 25.8–38 kV-Outdoor
|
Frame Width (X) |
||
|---|---|---|
|
29.50 in. (750 mm) |
39.37 in. (1000 mm) |
|
|
Bolt Center (Y) |
Add 2.25 in. (57 mm) to the total length of the switchgear lineup |
|
|
Unfused Switch |
1010 lb. (460 kg) |
1165 lb. (530 kg) |
|
Fused Switch |
1060 lb. (480 kg) |
1220 lb. (553 kg) |
|
Transition/Auxiliary Unit |
680 lb. (310 kg) |
830 lb. (375 kg) |
|
VT Compartment |
1450 lb. (650 kg) |
1600 lb. (725 kg) |
|
CT Compartment |
1400 lb. (634 kg) |
1545 lb. (700 kg) |
DANGER
WARNING