Assembling the Sub-Feed Circuit Breaker Deadfront Assembly
DANGER |
|---|
|
hazard of electric shock, explosion, or arc flash
Failure to follow these instructions will result in death or serious injury.
|
-
Remove the line and load end deadfront covers from the deadfront assembly. Discard the 10-32 x 7/16-in. mounting screws and deadfront covers.
-
Mount the line end deadfront cover using two 10-32 x 7/16-in. mounting screws supplied in the kit. Refer to Deadfront Cover Selection (below) for deadfront cover selection.
NOTE: Place the line end deadfront cover and the branch circuit breaker cover based on the top feed or bottom feed orientation.Deadfront Cover Selection
Circuit Count Cover Length Dimension A 30 13.08 in. (332.23 mm) 42 13.08 in. (332.23 mm) 54 16.05 in. (255.27 mm) 72 16.05 in. (255.27 mm) 84 16.05 in. (255.27 mm) -
Assemble the circuit breaker deadfront cover onto the deadfront extension supplied in the kit and install onto the deadfront assembly using the new 1032 x 7/16-in. mounting screws, also supplied in the kit. Install the circuit breaker escutcheon by pressing it against the circuit breaker deadfront cover and snap it into place.
DANGER