80043-867-01

Removing the Studs from the Elevating Brackets

For NQ Panelboards for Sub-Feed Circuit Breakers MH86D9 and MH92D9

  1. Unscrew the nuts from the stud welded in the box; studs welded in the box should remain.

  2. Remove the elevating brackets A and B.

  3. Unscrew the nut to remove the top stud.

  4. Remove the loosened top studs. Do not remove studs that are welded in the box.

  5. Place the elevating bracket back into place.

  6. Tighten the nuts back onto the studs welded in the box. Repeat as necessary for each stud.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?