80043-867-01

Reinstalling the Deadfront Assembly

  1. Reinstall the deadfront assembly using the screws retained when removing the deadfront assembly, and two additional 10-32 x 7/16-in. mounting screws supplied in this kit.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?