8501CT9601

Application Data

Average Operating Times In Milliseconds

Device Pick-Up Drop-Out
AC Relay 15 16
AC Latching Relay 15 13
DC Relay 37 21
DC latching Relay 37 45

Voltage Range:

AC operation, +10/-15%

DC operation, +10/-20%

In the case of dual rated DC coils, the range is +10% of the larger number and -20% of smaller number.

Operating Temperature Range:

-40°C to +71°C

-40°F to +160°F

Contact Ratings

Top of Cartridge AC Ratings
Volts Inductive 35% Power Factor Resistive 75% Power Factor
NEMA Rating Make Break Continuous Amperes Make, Break and Continuous Amperes
Amperes VA Amperes VA
Standard 120 A600 60 7200 6 720 10 10
240 30 7200 3 720 10 10
480 15 7200 1.5 720 10 10
Overlapping 600 12 7200 1.2 720 10 10
Master* A600 Same as standard cartridge above except substitute 20 Ampere for the continuous Ampere rating
 
 
Logic Reed 150 Vac, 150MA, 8W Maximum
Top of Cartridge DC Ratings
Volts Inductive Resistive
NEMA Rating Max. Make and Break Amperes (138VA Max. for 300 V or Less) Continuous Amperes Make and Break Amperes Continuous Amperes
 
Standard 125 P600 1.1 5 4 5
250 0.55 5 0.8 5
301–600 0.20 5
Overlapping 125 P150 1.1 5 4 5
Master* 125 P600 1.1 5 4 5
250 0.55 5 0.8 5
301–600 0.20 5
Logic Reed 30 Vdc, 60MA

Contact Arrangement

The following tables list all pole arrangements and the location of the N.O. and
N.C. poles. Relays purchased from the factory will correspond to these tables. For example: an XO12 will have one N.O. pole in position 1; positions 2 and 3 will have N.C. poles; position 4 will be a space.

NOTE: For additional information regarding contact cartridges see Pages 9 and 10.

2, 3, and 4–Pole Relay—All contacts convertible

No. of Poles Type Pole Number*
1 2 3 4
2

XO20

S O O S

XO11

S O 1 S

XO02

S 1 1 S
3

XO30

O O O S

XO21

O 1 O S

XO12

O 1 1 S

XO03

1 1 1 S
4

XO40

O O O O

XO31

O 1 O O

XO22

O 1 1 O

XO13

O 1 1 1

XO04

1 1 1 1

6 and 8–Pole Relay—All contacts convertible

No. of Poles Type Pole Number*
5 6 7 8
1 2 3 4
6

XO60

S O O S
O O O O

XO51

S O O S
O 1 O O

XO42

S O O S
O 1 1 O

XO33

S 1 1 S
O 1 O O

XO24

S 1 1 S
O 1 1 O

XO15

S 1 1 S
O 1 1 1

XO06

S 1 1 S
1 1 1 1
8

XO80

O O O O
O O O O

XO71

O 1 O O
O O O O

XO62

O 1 1 O
O O O O

XO53

O 1 O O
O 1 1 O

XO44

O 1 1 O
O 1 1 O

XO35

O 1 1 1
O 1 1 O

XO26

O 1 1 O
1 1 1 1

XO17

O 1 1 1
1 1 1 1

XO08

1 1 1 1
1 1 1 1

10 and 12–Pole Relay—All contacts convertible

No. of Poles Type Pole Number*
9 10 11 12
5 6 7 8
1 2 3 4
10

XO1000

S O O S
O O O O
O O O O

XO901

S O O S
O 1 O O
O O O O

XO0802

S O O S
O 1 1 O
O O O O

XO0703

S O O S
O 1 1 O
O 1 O O

XO0604

S O O S
O 1 1 O
O 1 1 O

XO0505

S O O S
O 1 1 O
O 1 1 O

XO0406

S 1 1 S
O 1 1 O
O 1 1 O

XO0307

S 1 1 S
O 1 1 1
O 1 1 O

XO0208

S 1 1 S
O 1 1 O
1 1 1 1
8 N.C. Poles Maximum
12

XO1200

O O O O
O O O O
O O O O

XO1101

O 1 O O
O O O O
O O O O

XO1002

O 1 1 O
O O O O
O O O O

XO0903

O 1 1 O
O 1 O O
O O O O

XO0804

O 1 1 O
O 1 1 O
O O O O

XO0705

O 1 1 O
O 1 1 O
O 1 O O

XO0606

O 1 1 O
O 1 1 O
O 1 1 O

XO0507

O 1 1 O
O 1 1 O
O 1 1 1

XO0408

O 1 1 O
O 1 1 O
1 1 1 1
8 N.C. Poles Maximum

Control Relay*

XTD and XTE Timer Attachments—All contacts convertible

No. of Poles Timed Contacts Type Pole Number*
13 14
2

XTD

O 1

XTE

Replacement AC Magnet Coils For Relays

Equipment to be serviced Coil Prefix or Class and Type Hz Suffix Number
(Complete Coil Number consists of Prefix or Class and Type followed by Suffix Number)
Coil Volt-Amperes
Class Type Poles 24 Volts 110–115 Volts 120 Volts 208 Volts 220 Volts 240 Volts 277 Volts 380 Volts 440 Volts 480 Volts 550 Volts 600 Volts Inrush Sealed
8501 X All 9998-X 60 23 44 51 52 53 55 62 65 148 23
50 24 44 52 53 62 65 143 25

Replacement DC Magnet Coils For Relays

Equipment to be serviced Coil Prefix or Class and Type Suffix Number
(Complete Coil Number consists of Prefix or Class and Type followed by Suffix Number)
Coil Burden Watts
Class Type Poles 6 Volts 12 Volts 18 Volts 24 Volts 32 Volts 48 Volts 64 Volts 72 Volts 90 Volts 110 Volts 115/125 Volts 220 Volts 230/250 Volts
8501 XD All 9998 XD 19 28 34 37 40 46 49 52 55 58 67 18
XDL 9998 XDL 19B 28B 34B 37B 40B 46B 49B 52B 55B 58B 67B 50
XUD All 9998 XUD 19 28 37 46 58* 67* 16

Definition of Ratings

Control relays are designed for switching inductive and resistive loads in both AC and DC circuits. By far, the greatest number of applications involve the switching of inductive loads in AC circuits. Typical loads include solenoids and operating coils of such devices as other relays, timers, starters and contactors.

The magnets on AC devices exhibit an inrush current when first switched on, with the current subsiding to some lesser value, known as the sealed current, after the magnet has moved to its sealed position. DC devices do not have an inrush current when first energized. Relay contacts may also be called upon to carry current continuously for long periods of time. This has resulted in recognizing three important ratings for relay contacts: the make rating, break rating and the continuous current rating. In addition, ratings are further divided into categories which depend upon whether the load is resistive or inductive in nature.

Contact Ratings

Contact Ratings on shows current and VA (volt-ampere) values in sufficient detail for most applications. A short definition of some of the terms used in the table follow:

  • Resistive Rating - Indicates the resistive load that the contacts can make, break or carry continuously. Resistive ratings are based on a 75% power factor.

  • Inductive Rating - Refers to loads such as coils of contactors, starters and relays and solenoids that contacts can make, break and carry continuously. Inductive rating tests are run with 35% power factor load.

  • Make Rating - Applies to the current that can be han-dled by the contact at the time of contact closure. In in-ductive AC circuits, the momentary inrush current is often 10 times the sealed current, and a relay must be able to handle this inrush current as well as be able to break it in an emergency. The endurance test listed in NEMA Standard ICS 5-1993 Paragraph 8 requires relay contacts to make the make rating for 6,000 operations.

  • Break Rating - Refers to the current that can be interrupted successfully by the contact. The inductive break rating is always less than the resistive or continuous ratings. When contacts break an inductive circuit, the inductance of the load tends to maintain the current. The result is an arc across the contacts which causes heating and erosion of the contacts. Because of the extra heat generated, the allowable inductive current must be less than the resistive current for equal contact life. The endurance test from NEMA Standard ICS 5-1993 Paragraph 8 requires relay contacts to interrupt the break rating for 6,000 operations. It also requires relay contacts to interrupt the make rating for 6 operations in an emergency.

  • Continuous Rating - Continuous rating indicates the load that the contacts can carry continuously without making or breaking the circuit and without exceeding a certain temperature rise.

Contact Life

The life of control relay contacts depends upon the magnitude and characteristics of the electrical load, inductance, duty cycle, mechanical properties of the device in which they are used, voltage fluctuations, environment, etc. The Class 8501 Type X relay carries a NEMA A600 rating. NEMA A600 relays have 600 VAC spacings, a 10 ampere continuous rating, a 60 ampere make rating, and a 6 ampere break rating at 120 volt AC for an AC inductive load.

When control circuit relays are operated at maximum rated load, the life of the contact is usually less than that of the mechanical life of the device. If the application requires a large number of operations during the life of the contacts, the contacts must be applied at values less than their maximum make and break ratings. NEMA Standard ICS 5-1993 Paragraph 8 recommends that control relays for automatically-operated sequencing systems be utilized with loads of less than 25% of the 60 ampere make and 6 ampere break ratings. It does not recommend using a relay at its maximum ampere rating where the number of operations are expected to substantially exceed the 6000 operations required by the endurance test in NEMA Standard ICS 5-1993 Paragraph 8.

Life-Load Guide

The information shown is provided to estimate the service life of a Class 8501 Type X control relay. This information is not to be taken as a guarantee, but rather an approximate life expectancy. The information is based on the following:

  • Operating 40 hours per week

  • Operating 52 weeks per year

  • Inrush and continuous current ratings not exceeded • Application in usual service conditions (such as described in NEMA Standard ICS 1-1993 Paragraph 6)

  • Operating at 120 Volts 60 Hertz

Service Life vs. Break Current

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.