8501CT9601

Accessories

Order Information

    Class 8501 Type  
Mechanical Latch Attachment – Mounts on any 2 through 8 pole relay (except XMO master relay). The Type XL and XDL latch attachments are identical in size and mounting provisions. The Type XL AC latch attachment has a continuous-duty-rated coil which is replaceable. The Type XDL DC latch attachment has an intermittent–rated coil (replaceable) and should be con-nected through a N.O. contact of the basic relay if the input signal is maintained to the unlatch coil.
  AC Latch Attachment

XL Mechanical Latch Attachment Voltage Codes:

File
CCN
E78403
NKCR2
File
Class
LR 60905
3211 02

  DC Latch Attachment

XDL Mechanical Latch Attachment Voltage Codes:

Pneumatic Timer Attachment – Mounts on any 0 through 4 pole AC or DC relay (except XMO master relay). It provides 1 N.O. and 1 N.C. convertible timed contacts, which are the same Type XC-1 cartridges used on the basic relay. Two timing ranges are available, and conversion from On Delay to Off Delay or vice versa is easy.
  Off Delay
 0.2–60 seconds
 5–180 seconds

XTD1


XTD2

File
CCN
E78403
NKCR2
File
Class
LR 60905
3211 02

  On Delay
 0.2–60 seconds
 5–180 seconds

XTE1


XTE2

Timer Lockout Cover – Fits over the time delay adjustment knob of any Type XT timing attachment. The Lockout Cover is designed to protect the time setting against accidental adjustment. It mounts directly to the timing attachment with two included screws.

XJ1

Adder Decks – Adder decks are used to expand the number of poles on a relay. The basic 4 pole relay can be easily converted to an 8 pole or 12 pole relay by installing one or two adder decks. The Class 8501 Type XB20 comes with 2 convertible contact cartridges and will accept 2 additional convertible contact cartridges. The Class 8501 Type XB40 comes with 4 convertible contact cartridges. The same Type XB adder deck is used for both the middle and upper decks of the AC or DC relay.
  With 2 N.O. contact cartridges

XB20

File
CCN
E78403
NKCR2
File
Class
LR 60905
3211 02

  With 4 N.O. contact cartridges

XB40

Logic Reed Adder Deck – Used for switching low energy circuits. The Logic Reed Adder Deck is supplied with either one or two logic reed cartridges fixed into the center positions of an adder deck. Contact cartridges are neither convertible nor replaceable. Standard cartridges can be inserted in unused cavities of the Logic Reed Adder Deck. One or two Logic Reed Adder Decks may be added to the basic 4 pole relay. See Application Data on Page 5 for electrical ratings. Number of N.O. Logic Reed Contact Cartridges Number of N.C. Logic Reed Contact Cartridges  

File
CCN
E78403
NKCR2
File
Class
LR 60905
3211 02

2 0

XBR20

1 1

XBR11

1 0

XBR10

0 1

XBR01

0 2

XBR02

Contact Cartridges – The Type X relay offers 4 Types of contact cartridges. All are color–coded for visual identification of each Type.
NOTE: For additional information regarding contact cartridge see Product Data.
 

File
CCN
E78403
NKCR2
File
Class
LR 60905
3211 02

Standard Cartridge – The standard cartridge, used for most applications, has a black case.

XC1

Overlapping Cartridge – Same NEMA Type A600 AC rating as standard cartridge and a NEMA Type P150 DC rating. When it is used in the N.O. mode it will close early and when used in the N.C. mode it will open late. If two or more are used together, the N.O. contacts will close before the N.C. contacts open as the relay picks up. Overlap also occurs during dropout. Overlapping cartridge has a red case.

XC2

  May be ordered factory installed:
 Substitute 1 N.O. and 1 N.C. overlapping cartridges for 2 standard cartridges.
 Substitute 2 N.O. and 2 N.C. overlapping cartridges for 4 standard cartridges.
Form
Y1591
Y1592
Master Cartridge – Features the same contact ratings as the Type XC1 standard cartridge except it has a 20 Ampere continuous current rating instead of 10 Amperes. It can be used in circuits where a master relay is required. Master cartridge has a blue case. Maximum of 6 master cartridges may be used on any 7 and 8 pole AC relays. Do not use any master cartridges on 9-12 pole AC or any DC-operated devices.

XC4

Logic Reed Cartridge – See Logic Reed Adder Deck above.
Mounting Track – The mounting track has pre-punched mounting holes to simplify mounting the track on the control panel. The relay mounting screws are factory installed on the track so that the relays can be hung prior to tightening the screws.
  9'' long for 4 relays

XM4

  18'' long for 8 relays

XM8

  27'' long for 12 relays

XM12

  36'' long for 16 relays

XM16

  72'' long for 32 relays

XM32

Manual Test Tool – Provides a means of manually switching the contacts of a basic relay or timing relay and holding all contacts in their switched state until the tool is removed. This simplifies the checking of control circuits without power on the coil or contacts.

XA1

File
CCN
E78403
NKCR2
File
Class
LR 60905
3211 02

Transient Suppressor – Consists of an R-C circuit designed to suppress coil generated transients to approximately 200 percent of peak voltage. It is particularly useful when switching the Type X relay near solid state equipment. It is designed for use on coils up to 120 Vac.

XS1

NEMA Type 1 Enclosure – Formed from sheet steel to provide strength and rigidity. Two conduit knockouts are located in both the top and bottom of the enclosure. The enclosure is furnished with self tapping screws for mounting the relay inside the enclosure. Accom-modates a single 4 or 8-pole AC or DC relay, 12-pole AC relay, 4-pole AC latching relay, and 4-pole AC timing relay.
NOTE: The 4-pole DC latching relay, 4-pole DC timing relay, 8-pole AC and DC latching relays and 12-pole Utility Auxiliary Relay will not fit.
Class 9991
Type UE7

File
CCN
E78403
NKCR2

Mechanical Latch Attachment Voltage Codes:

AC Voltages Code DC Voltage Code
24–60 V01 6 V50
24–50 V12 12 V51*
120–60 / 110–50 V02 18 V99
208–60 V08 24 V53
240–60 / 220–50 V03 48 V56
277–60 V04 72 V58
480–60 / 440–50 V06 90 V59
600–60 / 550–50 V07 115 / 125 V62
230 / 250 V66

For Replacement Coils see Replacement AC Magnet Coils For Relays or Replacement DC Magnet Coils For Relays.

How to Order:

To Order Specify: Catalog Number
  • Class Number

  • Type Number

  • Voltage Code for mechanical latch attachment

  • Form for factory installed overlapping contacts

  Class   Type  
  8501   XTE1  
         
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.