Ping Meters in ArcMap

There are two ways to ping meters in ArcMap:

  • Ping downstream of a chosen device.

  • Ping a group of selected meters.

Both methods initiate the ping procedure, and results are reported in Responder Explorer > Ping Requests tab.

IMPORTANT: Both ping tools do not appear on the Responder toolbar by default. Use Customize Mode to search for the tools and drag and drop them onto your toolbar.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?