Create Relationship Classes
The following relationship classes must be created in your geodatabase as part of Conduit Manager's minimum configuration requirements.
When building a relationship, the ArcCatalog relationship wizard wants to know where to find the unique identifier for the parent (that’s the primary key) and where this same identifier is placed in the child (that’s the foreign key). The application is then able to “match” the parent and child because all the children have the parent’s unique identifier. For the primary and foreign keys, Conduit Manager supports using ObjectID or GlobalID except for the Conduit_CrossSectionAnnotation relationship, which does not support GlobalID. This is because feature linked annotation relationships cannot be globalized.
The tables below are for new relationships. If you have existing relationships that you need to convert from ObjectID-based to Global-ID based, see the topic Migrate Existing Relationships to use GlobalID.
Conduit_CrossSectionAnnotation
For the primary and foreign keys, Conduit Manager supports either ObjectID or GlobalID except for the Conduit_CrossSectionAnnotation relationship, which does not support GlobalID. This is because feature linked annotation relationships cannot be globalized.
|
Origin table |
Conduit feature class |
|
Destination table: |
Cross Section Annotation feature class |
|
Relationship type: |
Composite (when conduit is deleted, associated annotation is deleted) |
|
Notification: |
None (no messages propagated)
IMPORTANT: The default notification for Composite
relationships is Forward. Ensure you change this to None.
|
|
Cardinality: |
One to Many |
|
Attributes? |
No |
|
Primary Key: |
ObjectID |
|
Foreign Key: |
FeatureID |
Conduit_Cable
Create a relationship between each conductor (or cable) class and the conduit feature class. For example:
-
Conduit_PriUGElectricLineSegment
-
Conduit_SecUGElectricLineSegment
-
Conduit_FiberOpticCable
|
Origin table: |
Conduit feature class |
|
Destination table: |
Conductor (Cable) feature class |
|
Relationship type: |
Simple |
|
Notification: |
None (no messages propagated) |
|
Cardinality: |
Many to Many |
|
Attributes? |
Yes |
|
Add fields: |
You must enter these three field names exactly as shown. Field model names are not supported in attributed relationships; thus, the application is looking for these fields exactly as they are displayed.
|
|
Origin (Conduit) Primary Key: |
ObjectID or GlobalID |
|
Destination (Conductor or Cable) Primary Key: |
ObjectID or GlobalID |
|
Origin (Conduit) Foreign Key: |
Conduit_ObjectID or Conduit_GlobalID This becomes the field name visible in the relationship table. Thus, we recommend adding a descriptor (for example, Conduit_ as seen above) so you know which ID is from the origin. The descriptor is up to you, but ensure it is recognizable for all GIS administrators. |
|
Destination (Conductor or Cable) Foreign Key: |
Cable_ObjectID or Cable_GlobalID This becomes the field name visible in the relationship table. Thus, we recommend adding a descriptor (for example, Cable_ as seen above) so you know which ID is from the destination. The descriptor is up to you, but ensure it is recognizable for all GIS administrators. |
Conduit_UGStructure
Create a relationship between each underground structure feature class and the conduit feature class.
|
Origin table: |
Conduit feature class |
|
Destination table: |
Underground Structure feature class |
|
Relationship type: |
Simple |
|
Notification: |
None (no messages propagated) |
|
Cardinality: |
Many to Many |
|
Attributes? |
No |
|
Origin (Conduit) Primary Key: |
ObjectID or GlobalID |
|
Destination (UGStructure) Primary Key: |
ObjectID or GlobalID |
|
Origin (Conduit) Foreign Key: |
Conduit_ObjectID or Conduit_GlobalID This becomes the field name visible in the relationship table. Thus, we recommend adding a descriptor (for example, Conduit_ as seen above) so you know which ID is from the origin. The descriptor is up to you, but ensure it is recognizable for all GIS administrators. |
|
Destination (UGStructure) Foreign Key: |
UGStructure_ObjectID or UGStructure_GlobalID This becomes the field name visible in the relationship table. Thus, we recommend adding a descriptor (for example, UGStructure_ as seen above) so you know which ID is from the destination. The descriptor is up to you, but ensure it is recognizable for all GIS administrators. |