Using Feeder Sync with Geodatabase Manager (GDBM)
- Configure the Feeder Sync Tool via the Feeder Manager Configuration window.
-
Add the following Action Handlers for the Feeder Sync Tool
to your existing GDBM configuration (see the Tasks topic for more information):
-
Run Feeder Sync assigned to Before Post.
-
Cleanup Feeder Sync assigned to After Post.
-
- Once GDBM has been properly configured for the Feeder Sync Tool, open ArcMap and create a new Session or Design.
-
Perform typical editing operations (create/delete features,
editing existing features, etc.) in that session or design.
-
Notice that the Feeder Information fields from Feeder Manager 2.0 update after each edit (Feeder IDs, Subfeeder IDs (if applicable), Energized Phases, Number of Feeders, Loop, Tie Device).
-
Notice that the Feeder Information in the legacy fields (FeederID, FeederID2 and FeederInfo) does not update after each edit.
-
- Save the session or design. This populates the MM_EDITED_FEATURES table. You can add the MM_EDITED_FEATURES table to inspect its contents if necessary.
- Send the Session or Design to the GDBM Post Queue.
- After GDBM runs through the posting process you can inspect the Logging tab for information on the number of features synced and if it was completed successfully.
- Open your SDE.Default version in ArcMap and inspect the legacy FeederID, FeederID2, and FeederInfo fields to see that they have been updated.