Create Relationships
Create the following relationships. If you are using the sample data, these may already exist. UFM also requires the Conduit_Conductor relationship. This should have been created in the basic configuration for Conduit Manager.
When building a relationship, the ArcCatalog relationship wizard wants to know where to find the unique identifier for the parent (that’s the primary key) and where this same identifier is placed in the child (that’s the foreign key). The application is then able to “match” the parent and child because all the children have the parent’s unique identifier. For the primary and foreign keys, Conduit Manager supports using ObjectID or GlobalID except for the Conduit_CrossSectionAnnotation relationship, which does not support GlobalID. This is because feature linked annotation relationships cannot be globalized.
The tables below are for new relationships. If you have existing relationships that you need to convert from ObjectID-based to Global-ID based, see the topic Migrate Existing Relationships to use GlobalID.
Conduit_DuctBank
|
Origin table: |
Conduit feature class |
|
Destination table: |
DuctBank feature class |
|
Relationship type: |
Simple |
|
Notification: |
None |
|
Cardinality: |
One to Many |
|
Attributes? |
No |
|
Primary Key: |
ObjectID or GlobalID |
|
Foreign Key: |
ObjectID or GlobalID |
PriUGElectricLineSegment_Duct
|
Origin table: |
PriUGElectricLineSegment |
|
Destination table: |
Duct |
|
Relationship type: |
Simple |
|
Notification: |
None |
|
Cardinality: |
Many to Many |
|
Attributes? |
Yes |
|
Fields to Add: |
PhaseDesignation (long integer) Cables (long integer) You must enter these two field names exactly as shown. Field model names are not supported in attributed relationships; thus, the application is looking for these fields exactly as they are displayed. |
|
Origin (Conductor) Primary Key: |
ObjectID or GlobalID |
|
Destination (Duct) Primary Key: |
ObjectID or GlobalID |
|
Origin (Conductor) Foreign Key: |
PrimaryUG_ObjectID or PrimaryUG_GlobalID This becomes the field name visible in the relationship table. Thus, we recommend adding a descriptor (for example, PrimaryUG_ as seen above) so you know which ID is from the destination. The descriptor is up to you, but ensure it is recognizable for all GIS administrators. |
|
Destination (Duct) Foreign Key: |
Duct_ObjectID or Duct_GlobalID This becomes the field name visible in the relationship table. Thus, we recommend adding a descriptor (for example, Duct_ as seen above) so you know which ID is from the destination. The descriptor is up to you, but ensure it is recognizable for all GIS administrators. |
SecUGElectricLineSegment_Duct
|
Origin table: |
SecUGElectricLineSegment |
|
Destination table: |
Duct |
|
Relationship type: |
Simple |
|
Notification: |
None |
|
Cardinality: |
Many to Many |
|
Attributes? |
Yes |
|
Field to Add: |
PhaseDesignation (long integer) Cables (long integer) You must enter these two field names exactly as shown. Field model names are not supported in attributed relationships; thus, the application is looking for these fields exactly as they are displayed. |
|
Origin (Conductor) Primary Key: |
ObjectID or GlobalID |
|
Destination (Duct) Primary Key: |
ObjectID or GlobalID |
|
Origin (Conductor) Foreign Key: |
SecondaryUG_ObjectID or SecondaryUG_GlobalID This becomes the field name visible in the relationship table. Thus, we recommend adding a descriptor (for example, SecondaryUG_ as seen above) so you know which ID is from the destination. The descriptor is up to you, but ensure it is recognizable for all GIS administrators. |
|
Destination (Duct) Foreign Key: |
Duct_ObjectID or Duct_GlobalID This becomes the field name visible in the relationship table. Thus, we recommend adding a descriptor (for example, Duct_ as seen above) so you know which ID is from the destination. The descriptor is up to you, but ensure it is recognizable for all GIS administrators. |
FiberCable_Duct
|
Origin table: |
FiberOpticCable |
|
Destination table: |
Duct |
|
Relationship type: |
Simple |
|
Notification: |
None |
|
Cardinality: |
Many to Many |
|
Attributes? |
Yes |
|
Field to Add: |
PhaseDesignation (long integer) You must enter this field name exactly as shown. Field model names are not supported in attributed relationships; thus, the application is looking for this field exactly as it is displayed.
IMPORTANT:
|
|
Origin (FiberOpticCable) Primary Key: |
ObjectID or GlobalID |
|
Destination (Duct) Primary Key: |
ObjectID or GlobalID |
|
Origin (FiberOpticCable) Foreign Key: |
FiberCable_ObjectID or FiberCable_GlobalID This becomes the field name visible in the relationship table. Thus, we recommend adding a descriptor (for example, FiberCable_ as seen above) so you know which ID is from the destination. The descriptor is up to you, but ensure it is recognizable for all GIS administrators. |
|
Destination (Duct) Foreign Key: |
Duct_ObjectID or Duct_GlobalID This becomes the field name visible in the relationship table. Thus, we recommend adding a descriptor (for example, Duct_ as seen above) so you know which ID is from the destination. The descriptor is up to you, but ensure it is recognizable for all GIS administrators. |