Using Fiber Manager for the First Time

Before you begin using Fiber Manager , you must enable the Fiber Manager extension. Click Customize > Extensions, and then select Fiber Manager .

TIP: If the DXI toolbar appears grayed out and inactive on your map, the most common reason is because the extension is not checked.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?