Configure Multiple Devices in the Same Rack Slot

Rather than being constrained to only one component per rack position, Wavepoint supports the configuration of multiple components in a single rack position.

For example, if you have three devices in the same slot, without this optional configuration, Wavepoint stacks them on top of each other following its “best fit” approach outlined in the previous help topic:


With this additional configuration, you can control their position in the slot and their widths:


To take advantage of this functionality, read through the subsequent help topics that describe the fields and model names that need to be added, and read about the various width configuration choices.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?