Configure Relationships and Model Names

Because Wavepoint  is published from a map service with Fiber Manager  data, most of the relationships and model names covered in the subsequent topics were likely created during your Fiber Manager  implementation. However, where Fiber Manager  is a flexible data model, Wavepoint  is not, and thus you should still confirm the relationships and model names, and configure them if they are missing.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?