Stop ArcGIS Server Service

After successfully installing ArcGIS Desktop and ArcGIS Server (and verifying the website is running), you are almost ready to start installing ArcFM applications. But, before you install ArcFM Server, you must stop the ArcGIS Server service. You might encounter problems if you do not stop the ArcGIS Server service before installing ArcFM Server, and it is easier to stop it now, install ArcFM Server, and then restart the service.

  1. Log into your server machine.
  2. Access the Services dialog:
    1. Press the Windows key and then type “Services” to find the dialog.
    2. Or, press Ctrl+Shift+Esc to open Windows Task Manager, and from there navigate to the Services tab.
  3. Right-click ArcGIS Server and choose Stop.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?