Patch Locations and Racks
When you visit a patch location, Wavepoint provides two tabs: Details and Inside.
Details
Inside
The Inside tab contains a list of racks, active and passive devices, and splitters at that location:
Click the name of a rack, device, or splitter to open its view.
The Details tab appears in the left pane with more information about the component. To the right is the Ports tab that contains a representation of the component.
After clicking the component, you can:
- 
                     
Click the panel or device name to zoom to that portion of the rack.
 - 
                     
Use your mouse cursor to pan around the rack.
 - 
                     
Hover over a port to view more information including type, status, and circuits.
 
For example, the following image displays the view of patch panels on a rack:
And as another example, the following image displays a 1 x 4 Splitter:
Connection Report
In the Details tab, click the Connection Report 
 icon to view the fiber connections on both sides of the panel or
               device.
The Report displays the following information:
- 
                     
The cable and fiber strands connected to one side of the port.
 - 
                     
Whether or not a circuit is present on a fiber strand.
 - 
                     
The port number.
 - 
                     
The type of port.
 - 
                     
The connection on the other side of the port, in particular if a jumper
 or a terminator 
 is present. 
Ports
When you click a port, the left pane displays the same details for the port including type, status, and circuits.
After clicking a port, you can: