Map
Wavepoint provides intuitive navigation and querying tools in a lightweight basemap.
- 
               
The main toolbar is visible at all times:
- 
                     
: The Layers drop-down allows you to toggle
                        the map layers on and off. - 
                     
: The Center Map button centers the basemap
                        around the feature currently selected. - 
                     
: The Move to Current Location button uses
                        the GPS coordinates at your current, physical location to reposition
                        the map, which allows you to view network elements near you. - 
                     
: The Measure Tool button provides Distance
                        and Location measuring tools. - 
                     
: The Select Basemap button allows
                        you to choose the basemap displayed under your fiber feature classes. - 
                     
: The Toggle Legend button toggles the
                        legend on and off in the left pane. 
 - 
                     
 - 
               
Use the stacked plus/minus
 buttons
                  on the left side of the map to zoom in and out, or use your mouse
                  scroll wheel. - 
               
At any time, click a fiber feature to view its attributes.
- 
                     
The first click displays the fiber feature name and its high-level attributes. Click the name of the feature to open detailed connection information and graphical views.
IMPORTANT: When clicking point features such as splice points or patch locations, the Selection pane displays all fiber features that come together at that point. 
 -