Print

The Print button provides a printer-friendly view of the current display in Wavepoint.

It works whether you are viewing the map, fiber connections, or inside a location.

Once on the print preview, you can still navigate and reposition the map or display prior to printing.

In your browser's Page Setup, ensure the option to Print Background Colors and Images is checked (the name of the checkbox varies among browsers).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?