Products and Licenses
ArcFM Viewer for ArcGIS Engine and its compatible extensions provide varying levels of editing capabilities. The Redliner and Inspector extensions require ArcFM Viewer with ArcGIS Engine along with its valid licensing. However, these two extensions do not rely upon one another and may be used independently.
|
Capabilities Licenses |
Esri Licenses |
Capabilities |
|
|---|---|---|---|
|
Capabilities Viewer for ArcGIS Engine |
Capabilities Viewer for ArcGIS Engine |
Engine Runtime |
View and query |
|
Redliner |
Capabilities Viewer for ArcGIS Engine, Redliner extension |
Engine Runtime |
View, query, redline editing |
|
Inspector |
Capabilities Viewer for ArcGIS Engine, Engine Editor extension |
Engine Runtime |
View, query, redline editing, and non-spatial attribute editing |
|
Engine runtime, Geodatabase Update extension |
View, query, redline editing, and attribute editing for various types* of features |
* A Geodatabase Update Extension license is required from Esri in order to edit relationship classes, feature-linked annotation, dimension feature classes and custom feature classes.