Main Menu
The Main Menu provides access to the tools listed below. Some of the tools - such as Zoom Data - are also available on toolbars.
|
Menu |
Tool |
Description |
|---|---|---|
|
File |
Open MXD |
Click File > Open MXD to view an existing .mxd file. |
|
Add New Tab |
Click File > Add New Tab to add another Data View tab. You may select a different stored display for each Data View tab. |
|
|
|
Click File > Print to print the selected map display. |
|
|
View |
Dockable Tabs |
Use the View menu to display tabs: Locator Tool, Table of Contents, Selectable Layers, Selection, Locator Results. |
|
Zoom Data |
The Zoom Data flyout menu gives the user access to some of the Map Tools for navigating the map. Click View > Zoom Data and choose a tool from the flyout menu. |
|
|
Bookmarks |
ArcFM Viewer allows you to view existing bookmarks. Click View > Bookmarks and choose one from the list. ArcFM Viewer does not allow creation of bookmarks. They must be created using ArcMap and saved with a stored display. |
|
|
Selection |
Zoom to Selected Features |
Click this tool to zoom to the set of features that are currently selected. |
|
Clear Selected Features |
This tool removes all features from the Selection tab. It does NOT remove features from the map. |
|
|
Select by Feeder |
This tool allows you to identify and highlight a feeder or set of feeders on a map. |
|
|
Stored Displays |
Stored Displays |
Select a stored display from the list provided. System stored displays are shown first, followed by User stored displays. Stored display environments allow you to change a large number of parameters in one step, so that you can switch between different views for different purposes. |
|
Tools |
Options |
Set display options such as zoom buffer and highlight color. |
|
Window |
Window Toggle |
If you have multiple stored displays open on multiple tabs, the Window menu allows you to toggle between multiple maps or stored displays. |
|
Help |
Help |
Access the ArcFM Viewer online documentation in this menu. |