Gestures
The Gesture tool is enabled only on tablet
PCs. Use a stylus to select the Gesture tool on a tablet PC. Then
you may use the stylus to draw the gestures described below to execute
specific tools.
Available Gestures
|
Gesture |
Name |
Action |
Description |
|---|---|---|---|
|
Scratch out |
Clear Selection |
Make the strokes as horizontal as possible and draw at least three strokes. If the height of the gesture increases, the number of back and forth strokes also needs to increase. |
|
|
Triangle |
Zoom Out |
Draw the triangle counter-clockwise in a single stroke, without lifting the pen. Make sure that the top of the triangle points upward. Draw the triangle clockwise to zoom in. In both instances, the triangle must be 'open'. A 'closed' triangle selects features instead of zoom. |
|
|
Square |
Zoom In |
Draw the square starting at the upper left corner. Draw the square with a single stroke, without lifting the pen. |
|
|
Arrow left |
Previous Extent |
Do not draw the arrow in more than two strokes. Draw the arrow either in a single stroke or in two strokes, where one stroke is the line and the other is the arrow head. Single stroke arrows written with the head as a triangle are not supported. |
|
|
Arrow right |
Next Extent |
Do not draw the arrow in more than two strokes. Draw the arrow either in a single stroke or in two strokes, where one stroke is the line and the other is the arrow head. Single stroke arrows written with the head as a triangle are not supported. |
|
|
Up-Down |
Zoom Out |
Draw this gesture in a single stroke starting with the up stroke. Draw the two strokes as close as possible. |
|
|
Down-Up |
Zoom Out |
Draw this gesture in a single stroke starting with the down stroke. Draw the two strokes as close as possible. |
|
|
Caret |
Pan Up |
Draw both sides of this gesture with equal length and in a single stroke. Make sure the angle is sharp and that the point is not rounded to a curve. |
|
|
Inverted caret |
Pan Down |
Draw both sides of this gesture with equal length and in a single stroke. Make sure the angle is sharp and that the point is not rounded to a curve. |
|
|
Chevron-left |
Pan Left |
Draw both sides of this gesture with equal length and in a single stroke. Make sure the angle is sharp and that the point is not rounded to a curve. |
|
|
Chevron-right |
Pan Right |
Draw both sides of this gesture with equal length and in a single stroke. Make sure the angle is sharp and that the point is not rounded to a curve. |
|
|
Tap |
Click |
Performing the tap in a swift motion results in the least amount of slipping. |
|
|
Double-Tap |
Double-Click |
Double-tapping in a feature with the appropriate model name launches the Inspector tool (Inspector extension license required). |
|
|
Any closed shape (circle, blob, rectangle, etc.) |
Select |
Make sure it is fairly closed or that the lines cross at the end point. |
|