DUG_Smoke alarm AC_CLP-00

Maintenance and cleaning

A monthly inspection is recommended to help ensure the device is dust, dirt, and insect free. The device can be vacuumed (strongly recommended) or brushed with a soft brush to remove accumulated dust, dirt or kitchen grease. Apply a small amount of insect surface spray to a cloth and wipe around device(s) every 3 to 6 months to mitigate insect ingress..

IMPORTANT:
  1. Always test the device after cleaning, for more information refer testing the device .

  2. If necessary refer to the installation instruction for more information about installing the device.


NOTICE
EQUIPMENT MAINTENANCE INSTRUCTIONS
  • Test the device regularly to ensure its functionality and the battery is in good condition.
  • Replace the device after 10 years from the date of manufacturing.
  • Do not open the device casing or repair yourself. There are no serviceable parts inside.
Failure to follow these instructions can result in equipment damage.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.