DUG_Smoke alarm AC_CLP-00

Pairing device with auto scan

Pairing the device with auto scan automatically discovers the device when the corresponding device is powered on.
  1. Turn on the device by sliding the power switch to I position on the rare side.
  2. On the Home page, tap + > Auto scan > Confirm .
  3. Enable permissions to Access location and Wi-Fi for scanning device and tap Start scanning.
    NOTE: If you have multiple hubs, do Step 4 or proceed to Step 5.
  4. Tap Select hub and select the Wiser hub from the slide-up menu.
  5. Press the Setup/Reset button 3 times and wait for a few seconds until the device search is complete..
    The LED blinks yellow.
    TIP: If you want to pair multiple devices at once, perform step 5 on each device and wait for a few seconds for them to be detected.
  6. Tap Next (A) and select Smoke Alarm.
  7. Once the device is added successfully, tap Done.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.