DUG_Iconic Connected Switch 10AX_CLP-00

Creating a moment

A Moment allows you to group multiple actions that are usually done together. Using the Wiser app, you can create moments based on your needs (such as movie night).
  1. On the Home page, tap .
  2. Go to Moment > + to create a moment.
  3. Tap Edit name , enter the name of the moment (A) and tap Save.
    TIP: You can choose the cover image that represents your moment by tapping .

  4. In the Action section, tap Add task (B) to open the slide-up menu.
  5. In the Add task menu, you can do either or all of the following actions (C):
    • Run the device: select the devices that you want in a moment.
    • Select Automation: select the automation that you want to enable or disable.
    • Delay: set the delay time.
    NOTE: You can add one or more actions using .

  6. Tap Run the device > Iconic Switch > Switch to select either or all of the functions to add in the moment:
    • On: turns on the switch (D).
    • Off: turns off the switch (E).
    • Reverse Switch: toggle the last state of switch (F).

  7. Set all actions and tap Save.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?