DUG_Iconic Connected Switch 10AX_CLP-00

Resetting the device manually

You can reset the device to factory default manually.

Short press the push button three times (<0,5 s) and then long press the push button once (>10 s).

After 10 s, release the push button when the LED starts blinking red .

NOTE: For Zigbee device, after reset, the LED turns amber/orange indicating that device is ready for pairing.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.