DUG_Iconic Connected Switch 10AX_CLP-00

Setting up a schedule

The device can be fully controlled by schedule. Once the schedule is set, the device operates at a given time.
  1. In the device control panel, tap Schedule > Add Schedule to add a schedule.
  2. In Add Schedule menu, set the time (A).
    NOTE: The Schedule works according to the time zone where the device is located.
  3. Tap Repeat (B) to select the days you want to set the schedule.
  4. Tap Note (C), enter the note and tap Confirm.
  5. Tap the toggle switch (D) to turn on the Notification for the schedule. The app will send a notification that the scheduled task is executed at the scheduled time.
  6. Tap Switch (E) and select any option, On or Off.

  7. Tap Save.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.