DUG_Iconic Connected Switch 10AX_CLP-00

Pairing Bluetooth device manually

Using the Wiser app, you can pair the device with smartphone to access and control the device.
NOTE: When pairing the Bluetooth device with the Wiser app, be within a range of 8 to 10 m of the module. Range can be affected by wall thickness and construction materials.
  1. On Home page, tap + then tap .
  2. Short press the push-button 3 times (< 0,5 s). In the app, select Confirm and tap Start Configuration (A).

    NOTE: Enable permissions to nearby devices and Bluetooth for scanning the device.
  3. Tap to select and add the device from the list and then tap Next > Done.
    NOTE: The device can be paired with max. 8 smartphones. To pair an additional phone, you must unpair one of the existing phones. Refer managed paired phones.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?