DUG_Iconic Connected Switch 10AX_CLP-00

Switching on/off the device using app

By using the Wiser app, you can switch on/off the device.

On the Home page, tap the power button (A) to switch on/off.

TIP: You can also navigate to control panel of the device and tap to switch on/off. The control panel always shows the current state of the switch.
NOTE: During timer mode, the device automatically turns off after a specified period of time. Refer timer mode.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?