DUG_Iconic Connected Twin 10 A Socket_CLP-00

Pairing Zigbee device with auto scan

Pairing the device with auto scan automatically discovers the device when the corresponding device is powered on.

To pair the device with auto scan:
  1. On the Home page, tap +.
  2. Tap Auto scan > Confirm .
  3. Enable permissions to Access location and Wi-Fi for scanning device and tap Start scanning.
    NOTE: If you have multiple hubs, do Step 4 or proceed to Step 5.
  4. Tap Select hub and select the Wiser hub from the slide-up menu.
  5. Short-press the touch button three times.
    NOTE: Wait for a few seconds until the device search is complete.
    TIP: If you want to pair multiple devices at once, perform step 5 on each device and wait for a few seconds for them to be detected.
  6. Tap Next (A), select Iconic Socket.
  7. Once the device is added successfully, tap Done.
QR code for this page

Was this helpful?