Thermal Memory
Presentation
The thermal memory is the means to take into account temperature rise and cooling caused by changes in the flow of current in the conductors.
These changes may be caused by:
-
Repetitive motor starting
-
Loads fluctuating near the long-time protection settings
-
Repeated circuit-breaker closing on a fault.
Trip units without a thermal memory (contrary to bimetal strip thermal protection) do not react to the above types of overloads because they do not last long enough to cause tripping. However, each overload produces a temperature rise and the cumulative effect can lead to dangerous overheating.
Trip units with a thermal memory record the temperature rise caused by each overload, even those that are very short. This information stored in the thermal memory reduces the tripping time.
MicroLogic Trip Units and Thermal Memory
All MicroLogic trip units are equipped as standard with a thermal memory.
For all protection functions, prior to tripping, the temperature-rise and cooling time constants are equal and depend on the tr time delay:
-
If the time delay is short, the time constant is low.
-
If the time delay is long, the time constant is high.
For long-time protection, following tripping, the cooling curve is simulated by the trip unit. Closing of the circuit breaker prior to the end of the time constant (approximately 15 minutes) reduces the tripping time indicated in the tripping curves.
Short-Time Protection and Intermittent Faults
For the short-time protection function, intermittent currents that do no provoke tripping are stored in the MicroLogic memory.
This information is equivalent to the long-time thermal memory and reduces the time delay for the short-time protection.
Following a trip, the short-time tsd time delay is reduced to the value of the minimum setting for 20 seconds.
Ground-Fault Protection and Intermittent Faults
The ground-fault protection implements the same intermittent fault function as the short-time protection.