DOCA0217EN-00

Presentation

PacT Series Master Range

Future-proof your installation with Schneider Electric’s low-voltage and medium-voltage PacT Series. Built on legendary Schneider Electric innovation, the PacT Series comprises world-class circuit breakers, switches, residual current devices and fuses, for all standard and specific applications. Experience robust performance with PacT Series within the EcoStruxure-ready switchgear, from 16 to 6300 A in low-voltage and up to 40.5 kV in medium-voltage.

Introduction

ComPacT NS630-3200 circuit breakers are equipped with a MicroLogic trip unit designed to help protect power circuits and connected loads.

X : Type of protection

  • 2 for basic protection

  • 5 for selective selection

  • 6 for selective + ground-fault protection

Y : Version number

Identification of the trip unit generation (0 is the first generation.)

Z : Type of measurement

  • A : Ammeter

  • E : Energy meter

  • P : Power meter

  • No indication : No measurements

Range of MicroLogic Trip Units

The following table indicates the functions available on ComPacT NS circuit breakers with MicroLogic trip units:

 

MicroLogic 2.0

MicroLogic 5.0

MicroLogic 6.0

Long-time overcurrent protection (L)

Short-time overcurrent protection (S)

Instantaneous overcurrent protection (I)

Ground-fault protection (G)

Neutral protection on 4P circuit breakers

Overload LED

Trip cause indicators

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.