DOCA0217EN-00

MicroLogic Trip Unit Description

MicroLogic 2.0 Trip Unit

  1. Top fastener

  2. Lead seal fixture for protective cover

  3. Connection with circuit breaker

  4. Bottom fastener

  5. Protective cover

  6. Cover opening point

  7. Long-time rating plug

  8. Screw for long-time rating plug

  9. Long-time current setting Ir

  10. Long-time time delay tr

  11. Short-time pickup Isd

  12. QR code on protective cover, to access product information

  13. Test connector

  14. Overload indication LED

MicroLogic 5.0 Trip Unit

  1. Top fastener

  2. Lead seal fixture for protective cover

  3. Connection with circuit breaker

  4. Bottom fastener

  5. Protective cover

  6. Cover opening point

  7. Long-time rating plug

  8. Screw for long-time rating plug

  9. Long-time current setting Ir

  10. Long-time time delay tr

  11. Short-time pickup Isd

  12. Short-time time delay tsd

  13. Instantaneous pickup Ii

  14. QR code on protective cover, to access product information

  15. Test connector

  16. Overload indication LED

MicroLogic 6.0 Trip Unit

  1. Top fastener

  2. Terminal block for external connections

  3. Housing for battery

  4. Lead seal fixture for protective cover

  5. Connection with circuit breaker

  6. Bottom fastener

  7. Protective cover

  8. Cover opening point

  9. Long-time rating plug

  10. Screw for long-time rating plug

  11. Long-time current setting Ir

  12. Long-time time delay tr

  13. Short-time pickup Isd

  14. Short-time time delay tsd

  15. Ground-fault pickup Ig

  16. Ground-fault time delay tg

  17. Test connector

  18. Test button for ground-fault protection

  19. Instantaneous pickup Ii

  20. Overload indication LED

  21. QR code on protective cover, to access product information

  22. Test/Reset button

  23. Auto-protection trip cause indication LED

  24. Ground-fault trip cause indication LED

  25. Short-time or instantaneous trip cause indication LED

  26. Long-time trip cause indication LED

Overload Indication LED

LED Description

Overload alarm: the load exceeds 105% of the Ir setting of the long-time protection.

QR Code

When the QR code on the protective cover of a MicroLogic trip unit is scanned with a smartphone running a QR code reader and connected to the Internet, the Go2SE landing page is displayed. The landing page displays some information about the device and a list of menus.

Sensor Plug

The protection ranges depend on the rated current In, defined by the sensor plug present below the MicroLogic trip unit.

Trip Cause Indication LED (MicroLogic 6.0)

LED Description

Trip due to long-time protection

Trip due to short-time protection or instantaneous protection

Trip due to ground-fault protection

Trip due to auto-protection

When activated, a LED remains ON until it is locally reset.

NOTE:
  • A number of simultaneous causes may result in tripping. The LED signalling the last trip cause chronologically is the only one to remain ON.

  • The battery maintains the trip cause indications. If there are no indications, check the battery.

Test Button for Ground-Fault Protection (MicroLogic 6.0)

The test button is used to test the ground-fault protection for MicroLogic 6.0 trip unit.

Test/Reset Button (MicroLogic 6.0)

Use the Test/Reset button to:

  • Reset the trip cause indications:

    1. Determine why the circuit breaker tripped. The trip cause indication is maintained until it is reset on the trip unit.

    2. Press the Test/Reset button.

    3. Check the parameter settings of the trip unit.

  • Check the battery: press the Test/Reset button to check the luminance of the trip cause indication LEDs. If the LEDs are dim, or not lit, change the battery.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.