Setting Procedure

  1. Open the protective cover.
  2. Make the necessary settings using the dials. The set value is automatically displayed on the screen in absolute value with the relevant units:
    • Current in amperes (A and kA).

    • Time delays in seconds.

    If no information is displayed, refer to MicroLogic Display.

  3. If no further action is taken, the display returns to the main menu for current measurements after a few seconds.
  4. Close the protective cover and, if necessary, install a lead seal to protect the settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?