Setting MicroLogic  6.0 A/E Trip Unit

You can set the tripping curve of your MicroLogic  6.0 A/E trip unit to match the needs of your installation using the following parameters:

  1. Current setting Ir (long time)

  2. Time delay tr (long time) for 6 x Ir

  3. Pickup Isd (short time)

  4. Time delay tsd (short time)

  5. Pickup Ii (instantaneous)

  6. Pickup Ig (ground fault)

  7. Time delay tg (ground fault)

Set the Threshold Values

In this example, the rated current In of the circuit breaker is 2000 A.

Ir = 0.7 x In = 1400 A

Isd =2 x Ir = 2800 A

Ii = 3 x In = 6000 A

Ig = 640A

I²t ON curve

I²t OFF curve

Set the Time Delays

In this example, time delay tr of the circuit breaker is 1 second, time delay tsd is 0.2 seconds, and time delay tg is 0.2 seconds.

I²t ON curve

I²t OFF curve

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?