DOCA0298EN-02

Locking the Device in Open Position with Keylocks

Description

Optional keylocks can be used:

  • To lock one EasyPact MVS2 device in the open position. When locked the device cannot be closed either locally with the closing pushbutton or remotely.

  • To interlock several EasyPact MVS2 device locked with the same key.

To use keylocks to lock the device in the open position, an optional OFF-position locking accessory is necessary.

VSPO OFF-Position Locking Accessory

The OFF-position locking accessory is an optional accessory that is mounted on the front of the device.

The OFF-position keylocking accessory can be fitted with one keylock.

The following types of keylocks can be fitted:

Ronis keylock

Profalux keylock

For information on the accessory installation, consult the instruction sheet on the Schneider Electric website: MVS21736.

Locking the Device in the Open Position

Step

Action

1

Press and hold the opening pushbutton.

2

With the opening pushbutton pressed, turn the key clockwise to lock the device.

3

Remove the key.

4

Release the opening pushbutton.

5

Check that the device is locked in the open position and cannot be closed either locally with the closing pushbutton or remotely.

Unlocking the Device

Step

Action

1

Put the key in the keylock.

2

Turn the key clockwise to unlock the device.

3

Press the closing pushbutton to close the device.

NOTE: The key remains captive in the keylock.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.