Firmware Update

Introduction

The primary reason for updating the firmware of a MicroLogic B/BPTS control unit trip system is to obtain the latest MicroLogic B/BPTS features. If the latest MicroLogic B/BPTS features are not required, it is not mandatory to update the firmware of the MicroLogic B/BPTS control unittrip system.

The standard protection functions of the MicroLogic B/BPTS control unittrip system is not active during a firmware update.

Use the latest version of EcoStruxure Power Commission software for all firmware updates.

For more information about firmware updates, refer to the DOCA0314EN MasterPacT MTZ - MicroLogic B/BP Control Units - Firmware Release Notes.DOCA0315EN EasyPact MVS - TS Trip System Firmware Release Notes.DOCA0316EN EasyPact EVS - TS Trip System Firmware Release Notes.

Checking the Firmware Version

Check the firmware version:

Updating Firmware With EcoStruxure Power Commission Software

WARNING
FIRE HAZARD
Put the circuit breaker in OFF position before starting the firmware update. During firmware update, the circuit breaker cannot provide protection.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
NOTICE
FIRMWARE UPDATE UNSUCCESSFUL
  • The MicroLogic B/BP control unit must be powered by USB during the firmware update.
  • Do not disconnect the function test and isolation module before clicking the CLOSE button at the end of the update procedure with EcoStruxure Power Commission software.
Failure to follow these instructions can result in equipment damage.
NOTICE
INTERRUPTION OF POWER SUPPLY
  • The TS trip system must be powered by USB during the firmware update.
  • Do not disconnect the function test and isolation module before clicking the CLOSE button at the end of the update procedure with EcoStruxure Power Commission software.
Failure to follow these instructions can result in equipment damage.

The prerequisites for updating the firmware with EcoStruxure Power Commission software are the following:

  • The latest version of EcoStruxure Power Commission software must be downloaded and installed on the PC.

  • The PC must be connected to a power supply. Standby mode must be deactivated to avoid the possibility of interruption during the update.

  • The PC must be connected to the 5-pin plug on the MicroLogic B/BPTS control unittrip system through a function test and isolation module (commercial reference LV910200SP).

The Administrator password of the MicroLogic B/BPTS control unittrip system is required to launch the firmware update.

NOTE: The protection functions are not active during MicroLogic B/BPTS firmware update.

For more information, refer to EcoStruxure Power Commission Online Help.

Predefined Events

The following events can be generated when a firmware update is performed:

Code

Event

History

Severity

0x1434 (5172)

Firmware self diagnostic error

Diagnostic

High

Predefined events cannot be modified by the user. For general information about events, refer to Event Management.

Recommended Actions

Code

Event

Recommended Actions

0x1434 (5172)

Firmware self diagnostic error

Update the firmware of the control unittrip system with EcoStruxure Power Commission software.

Contact your Schneider Electric Services representative for more information about who can carry out the recommended actions.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?