DOCA0299EN-03

EcoStruxure Power Device App

Presentation

EcoStruxure Power Device app is a single mobile application with the necessary information and capabilities to operate and efficiently maintain devices in the EcoStruxure architecture.

The application enables you to connect to devices, including the following:

  • EasyPact MVS circuit breakers

  • TeSys GV4 motor circuit breakers

  • Easergy P3 protection relays

The application can be installed on a smartphone by downloading from:

  • Google Play Store or other app stores in China for Android smartphones.

  • App Store for iOS smartphones.

EasyPact MVS Devices in EcoStruxure Power Device App

With the EcoStruxure Power Device app, a smartphone can be used with EasyPact MVS circuit breakers as the primary interface for day-to-day and critical case maintenance.

The TS trip system is identified on the application by scanning the QR code on the trip system.

Wireless communication is available by NFC communication.

Using an NFC Connection

Connecting to EcoStruxure Power Device app with an NFC connection is always possible, even when the TS trip system is not powered. For more information, refer to the NFC connection procedure.

It gives access to the following information:

  • Information about the TS trip system

    • Protection settings (display only)

    • Alarm indications

  • Last trip context: trip type; current values before trip

  • List of up to 5 active alarms

  • Real time measurements: current measurements, maximum currents, and unbalance current

  • Circuit breaker maintenance counters

    • Counter of electrical operations

    • Counter of trips

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?