DOCA0299EN-03

EcoStruxure Power Commission Software

Overview

EcoStruxure Power Commission software helps you to manage a project as part of testing, commissioning, and maintenance phases of the project life cycle. The innovative features in it provide simple ways to configure, test, and commission the smart electrical devices.

EcoStruxure Power Commission software automatically discovers the smart devices and allows you to add the devices for an easy configuration. You can generate comprehensive reports as part of Factory Acceptance Test and Site Acceptance Test to replace your heavy manual work. Additionally, when the panels are under operation, any change of settings made can be easily identified by a yellow highlighter. This indicates the difference between the project and device values, and hence provides a system consistency during the operation and maintenance phase.

The EcoStruxure Power Commission software enables the configuration of the EasyPact MVS circuit breakers with TS trip system.

For more information, refer to the EcoStruxure Power Commission Online Help.

Click here to download the latest version of EcoStruxure Power Commission software.

Key Features

EcoStruxure Power Commission software performs the following actions for the supported devices and modules:

  • Create projects by device discovery

    .
  • Save the project in the EcoStruxure Power Commission cloud for reference (not available in China)

    .
  • Upload alarms settings to the circuit breaker and download settings from the circuit breaker

    .
  • Set the alarm threshold

    .
  • Generate and print the circuit breaker settings report

    .
  • View the measurements, logs, and maintenance information

    .
  • View the status of the circuit breaker

    .
  • View the alarm details

    .
  • Check the system firmware compatibility status

    .
  • Update to the latest device firmware

    .
  • Perform force trip test, and automatic trip curve tests with preconfigured or custom test points

    .

TBD@experts:

Add topic about the EPC application/Mobile??????

The application can be installed on a smartphone by downloading the application

from:

??? China store for Android smartphones

??? China store for iOS smartphones

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?