Important Safety Instructions — SAVE THESE INSTRUCTIONS
Read these instructions carefully and look at the equipment to become familiar with it before trying to install, operate, service or maintain it. The following safety messages may appear throughout this manual or on the equipment to warn of potential hazards or to call attention to information that clarifies or simplifies a procedure.
|  DANGER | 
|---|
| DANGER indicates a hazardous situation which, if
                        not avoided, will result in death or serious injury. Failure to follow these instructions will result in death or serious injury. | 
|  WARNING | 
|---|
| WARNING indicates a hazardous situation which,
                        if not avoided, could result in death or serious injury. Failure to follow these instructions can result in death, serious injury, or equipment
                        damage. | 
|  CAUTION | 
|---|
| CAUTION indicates a hazardous situation which,
                        if not avoided, could result in minor or moderate injury. Failure to follow these instructions can result in injury or equipment damage. | 
| NOTICE | 
|---|
| NOTICE is used to address practices not related
                        to physical injury. The safety alert symbol shall not be used with
                        this type of safety message. Failure to follow these instructions can result in equipment damage. | 
Please Note
Electrical equipment should only be installed, operated, serviced, and maintained by qualified personnel. No responsibility is assumed by Schneider Electric for any consequences arising out of the use of this material.
A qualified person is one who has skills and knowledge related to the construction, installation, and operation of electrical equipment and has received safety training to recognize and avoid the hazards involved.
Per IEC 62040-1: "Uninterruptible power systems (UPS) -- Part 1: Safety Requirements," this equipment, including battery access, must be inspected, installed and maintained by a skilled person.
The skilled person is a person with relevant education and experience to enable him or her to perceive risks and to avoid hazards which the equipment can create (reference IEC 62040-1, section 3.102).
Safety Precautions
|  DANGER | 
|---|
| HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH Read all instructions in the installation manual before
                           installing or working on this product. Failure to follow these instructions will result in death or serious injury. | 
|  DANGER | 
|---|
| hazard of electric shock, explosion, or arc flash Do not install the product until all construction work
                           has been completed and the installation room has been cleaned. Failure to follow these instructions will result in death or serious injury. | 
|  DANGER | 
|---|
| HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH The product must be installed according to the specifications
                           and requirements as defined by Schneider Electric. It concerns in
                           particular the external and internal protections (upstream breakers,
                           battery breakers, cabling, etc.) and environmental requirements. No
                           responsibility is assumed by Schneider Electric if these requirements
                           are not respected. Failure to follow these instructions will result in death or serious injury. | 
|  DANGER | 
|---|
| HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH The UPS system must be installed according to local and
                           national regulations. Install the UPS system according to:
                            
 Failure to follow these instructions will result in death or serious injury. | 
|  DANGER | 
|---|
| hazard of electric shock, explosion, or arc flash 
 Failure to follow these instructions will result in death or serious injury. | 
|  DANGER | 
|---|
| hazard of electric shock, explosion, or arc flash The product is not designed for and must therefore not
                           be installed in the following unusual operating environments:
                            
 Failure to follow these instructions will result in death or serious injury. | 
|  DANGER | 
|---|
| Hazard of electric shock, explosion, or arc flash Do not drill or cut holes for cables or conduits with
                           the gland plates installed and do not drill or cut holes in close
                           proximity to the UPS system. Failure to follow these instructions will result in death or serious injury. | 
|  WARNING | 
|---|
| HAZARD OF ARC FLASH Do not make mechanical changes to the product (including
                           removal of cabinet parts or drilling/cutting of holes) that are not
                           described in the installation manual. Failure to follow these instructions can result in death, serious injury, or equipment
                           damage. | 
| NOTICE | 
|---|
| risk of overheating Respect the space requirements around the product and
                           do not cover the ventilation openings when the product is in operation. Failure to follow these instructions can result in equipment damage. | 
Additional Safety Precautions After Installation
|  DANGER | 
|---|
| hazard of electric shock, explosion, or arc flash Do not install the UPS system until all construction work
                              has been completed and the installation room has been cleaned. If
                              additional construction work is needed in the installation room after
                              this product has been installed, turn off the product and cover the
                              product with the protective packaging bag the product was delivered
                              in. Failure to follow these instructions will result in death or serious injury. | 
Electrical Safety
This manual contains important safety instructions that should be followed during the installation and maintenance of the UPS system.
|  DANGER | 
|---|
| hazard of electric shock, explosion, or arc flash 
 Failure to follow these instructions will result in death or serious injury. | 
The label below must be added if:
- 
                           The UPS input is connected through external isolators that, when opened, isolate the neutral, OR 
- 
                           The UPS input is connected via an IT power system. 
|  DANGER | 
|---|
| Hazard of electric shock, explosion, or arc flash Risk of voltage backfeed. Before working on this circuit:
                                 Isolate the UPS and check for hazardous voltage between all terminals
                                 including the protective earth. Failure to follow these instructions will result in death or serious injury. |