Important Safety Instructions — SAVE THESE INSTRUCTIONS
Read these instructions carefully and look at the equipment to become familiar with it before trying to install, operate, service or maintain it. The following safety messages may appear throughout this manual or on the equipment to warn of potential hazards or to call attention to information that clarifies or simplifies a procedure.
DANGER |
|---|
|
DANGER indicates a hazardous situation which, if not avoided, will result in death or serious injury.
Failure to follow these instructions will result in death or serious injury.
|
WARNING |
|---|
|
WARNING indicates a hazardous situation which, if not avoided, could result in death or serious injury.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
CAUTION |
|---|
|
CAUTION indicates a hazardous situation which, if not avoided, could result in minor or moderate injury.
Failure to follow these instructions can result in injury or equipment damage.
|
| NOTICE |
|---|
|
NOTICE is used to address practices not related to physical injury. The safety alert symbol
shall not be used with this type of safety message.
Failure to follow these instructions can result in equipment damage.
|
Please Note
Electrical equipment should only be installed, operated, serviced, and maintained by qualified personnel. No responsibility is assumed by Schneider Electric for any consequences arising out of the use of this material.
A qualified person is one who has skills and knowledge related to the construction, installation, and operation of electrical equipment and has received safety training to recognize and avoid the hazards involved.
Electromagnetic Compatibility
| NOTICE |
|---|
|
Risk of electromagnetic disturbance
This is a product Category C3 according to IEC 62040-2. This is a product for commercial
and industrial applications in the second environment - installation restrictions
or additional measures may be needed to prevent disturbances. The second environment
includes all commercial, light industry, and industrial locations other than residential,
commercial, and light industrial premises directly connected without intermediate
transformer to a public low-voltage mains supply. The installation and cabling must
follow the electromagnetic compatibility rules, e.g.:
Failure to follow these instructions can result in equipment damage.
|
Safety Precautions
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Read all instructions in the installation manual before installing or working on this
product.
Failure to follow these instructions will result in death or serious injury.
|
DANGER |
|---|
|
hazard of electric shock, explosion, or arc flash
Do not install the product until all construction work has been completed and the
installation room has been cleaned.
Failure to follow these instructions will result in death or serious injury.
|
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
The product must be installed according to the specifications and requirements as
defined by Schneider Electric. It concerns in particular the external and internal
protections (upstream breakers, battery breakers, cabling, etc.) and environmental
requirements. No responsibility is assumed by Schneider Electric if these requirements
are not respected.
Failure to follow these instructions will result in death or serious injury.
|
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
The UPS system must be installed according to local and national regulations. Install
the UPS according to:
Failure to follow these instructions will result in death or serious injury.
|
DANGER |
|---|
|
hazard of electric shock, explosion, or arc flash
Failure to follow these instructions will result in death or serious injury.
|
DANGER |
|---|
|
hazard of electric shock, explosion, or arc flash
The product is not designed for and must therefore not be installed in the following
unusual operating environments:
Failure to follow these instructions will result in death or serious injury.
|
DANGER |
|---|
|
Hazard of electric shock, explosion, or arc flash
Do not drill or cut holes for cables or conduits with the gland plates installed and
do not drill or cut holes in close proximity to the UPS.
Failure to follow these instructions will result in death or serious injury.
|
WARNING |
|---|
|
HAZARD OF ARC FLASH
Do not make mechanical changes to the product (including removal of cabinet parts
or drilling/cutting of holes) that are not described in the installation manual.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
| NOTICE |
|---|
|
risk of overheating
Respect the space requirements around the product and do not cover the ventilation
openings when the product is in operation.
Failure to follow these instructions can result in equipment damage.
|
Electrical Safety
DANGER |
|---|
|
hazard of electric shock, explosion, or arc flash
Failure to follow these instructions will result in death or serious injury.
|
Distribution-Related Backfeed
The upstream disconnection switchgear must be suitable for disconnection purposes. Before working on the upstream supply, the MBB must be locked in the open position using the built-in lockout function.
When installing the parallel maintenance bypass panel, warning labels must be posted on the load side of all upstream disconnection devices. The labels must be supplied by the user, displaying the following text (or equivalent in a language which is acceptable in the country in which the UPS system is installed):
DANGER
WARNING
CAUTION
DANGER
WARNING